AOUT#.VALUEU
Description
Gets or sets the user command value of the specified analog output when AOUT#.SOURCE = 0 (user).
Examples
Usage
When AOUT#.SOURCE = 0 (user) then the corresponding AOUT#.VALUEU is used to drive the AOUT#.VALUE .
Code
Changing output value with VALUEU and then changing SOURCE to be action table with no action configured:
--> AOUT1.SOURCE 0 //user --> AOUT1.VALUEU 0.000 V --> AOUT1.VALUE 0.000 V --> AOUT1.VALUEU 1 --> AOUT1.VALUE 1.000 V
Context
For more information see Analog Output.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
| Type | Read/Write |
| Units | V |
| Range | 0 to 10 |
| Default Value | 5 |
| Data Type | Float |
| See Also | |
| Stored in Non Volatile Memory | No |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO Mappable |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AOUT1.VALUEU | 0x3800 | 0x2 | INT | 1000:1 | - | RW | True |
| AOUT2.VALUEU | 0x3801 | 0x2 | INT | 1000:1 | - | RW | True |
|
Copyright © 2018 Kollmorgen |
|